Technical FAQs

Ask a Question

What to do if my UPS (SURT20KUXI) is showing "Runtime Is Below Alarm Threshold"?

Follow the steps,


Option 1) Allow the batteries to recharge.
Option 2) If possible, increase the number of battery modules.
Option 3) Reduce the load.
Option 4) Decrease the alarm threshold
Was this helpful?
What can we do to improve the information ?