Technical FAQs

Ask a Question

Version information does not update when virtual version of StruxureWare Central is upgraded.

Issue:

Version information does not update when virtual version of StruxureWare Central is upgraded.

Product Line:

StruxureWare Central/StruxureWare Data Center Expert

Environment:

Upgrade from the virtual version 7.0 of StruxureWare Central to version 7.2 StruxureWare Data Center Expert.

Resolution:

When upgrading from the virtual version 7.0 of StruxureWare Central to version 7.2 StruxureWare Data Center Expert, the version information that ESXI reports shows 7.0 instead of 7.2. In order to find the actual version, simply go to the Data Center Expert's help and about information. This will show the proper version information.
 
Was this helpful?
What can we do to improve the information ?