Netbotz SP155 readings are inaccurate with version 3.0.0 Botzware.
Product Line:
NetBotz
Environment:
Netbotz SP155
Cause:
Firmware issue
Resolution:
Upgrading to Botzware version 3.0.1 from version 3.0.0 should resolve any discrepancy in the readings of the SP155. This can be done through the Netbotz advanced view or through InfraStruXure Central.