Technical FAQs

Ask a Question

NetBotz v4.2 Web Client Does Not Run on IE8 or IE9 in Compatibility View


The NetBotz version 4.2 Web Client does not run on Internet Explorer 8 or Internet Explorer 9 when displayed in Compatibility View.

Product Line:



Microsoft Internet Explorer version 8.0
Microsoft Internet Explorer version 9.0
NetBotz version 4.2 Web Client


It is a known issue that the NetBotz v4.2 Web Client does not function with the browser set to display websites in Compatibility View.


Change the Compatibility View Settings in the browser.

For more information about Compatibility View, see the following Microsoft article:

This issue should be resolved with the release of 4.3
Was this helpful?
What can we do to improve the information ?