Technical FAQs

Ask a Question

Which devices are the Universal CD-Rom Sound Card Cable compatible with?

Issue:
Will the Universal CD Rom cable be compatible with my CD Rom and sound card?

Product Line:
Cables and Connectivity Solutions
 
Environment:
All versions and serial ranges.
 
Cause:
Customers need to be sure they purchase the correct CD Rom sound card cable
 
Resolution:
The Universal CD Audio Cable (P/N 76119) connects almost all sound cards to almost any CD Rom. The 4-pin black connector exists on almost every Sound Card. There are three connectors on the CD Rom end of this cable. One of these three connectors exists on almost every CDR or CDRW.

All APC brand Cables and Connectivity Solutions products like Cat 5E, Cat 6, Cat 6A patch cables, fiber optic cables, USB cables and adapters, Monitor cables, A/V cables, adapters and converters can be found at: www.apccables.com.
Was this helpful?
What can we do to improve the information ?