Technical FAQs

Ask a Question

NetBotz: Sending SMS Alerts as a Threshold Specific Notification.

Issue:

Sending SMS Alerts as a Threshold Specific Notification.

Product Line:

NetBotz

Environment:

NetBotz version 2

Cause:

Alternative notification method

Resolution:

To send a SMS message over the GSM network by using threshold specific address, simply put SMS:the phone number in the address field instead of an email address.

Example:
SMS:5125551234
 
Was this helpful?
What can we do to improve the information ?