Technical FAQs

Ask a Question

Configuring alarm thresholds for notification in StruxureOn


Issue
Configuring alarm thresholds for notification in StruxureOn

Product Line
StruxureOn

Environment
StruxureOn Gateway
StruxureOn smartphone app

Resolution

You will only receive alarm notifications on critical alarms occurring on Premium devices. There are default settings for criticality on most devices, but you can determine which alarms are critical by customizing alarm thresholds in the StruxureOn Gateway. Alarm thresholds can also be defined directly on a network management card (NMC) but if you're defining thresholds on multiple devices, it is easier to do in the StruxureOn Gateway.
  1. In the StruxureOn Gateway, go to More… > Alarm Configuration.
  2. Click Create Alarm Configuration, and choose a sensor type.
  3. Specify a name for the alarm configuration.
  4. Specify a value for at least one threshold parameter: Minimum, Low, High, or Maximum.
  5. Click Add sensor type.
  6. Filter the list by device type and device group. You can narrow the list using text you type to find only the sensors you want in the list.
  7. Click +Add or +Add all to include the sensors you want to respond the threshold alarm.
  8. Click Done and OK to finish the configuration.

When a monitored device sensor reports a value below what you defined as Low, it will generate an alarm with the severity of warning.
When a monitored device sensor reports a value below what you defined as Minimum, it will generate an alarm with the severity of critical.

Was this helpful?
What can we do to improve the information ?