Storage Temperature Range for All NetBotz Version Appliances
Issue:
Storage Temperature Range for version 1 and 2 NetBotz Appliances
Product Line:
NetBotz
Environment:
NetBotz version 1 and 2
Cause:
Storage Information
Resolution:
The following are the temperature ranges for storing NetBotz Appliances:
Model 310/400 = -25 C to 85 C
Model 320/420 = -10 C to 70 C*
Model 500 = -25 C to 85 C*
Note:*Humidity sensor re-hydrating times may be necessary after prolonged exposure to extreme high temperatures and low humidity. See the following article:
http://www.sensirion.com/en/pdf/Soldering_Procedure_SHT1x_en_v1.2.pdf