Technical FAQs

Ask a Question

Where do I find the setting for Celsius or Fahrenheit selection within the AP9631 NMC2 Card

Issue:
Unable to find location of the setting for Celsius or Fahrenheit selection for AP9631, RPDU2, and NetBotz 250
 

Product line:
AP9631
AP9631
RPDU2
NBRK0250
 

Environment:
5.x and 6.x firmware
 
 
Resolution:
Log into the NMC card and look at the top right side where you will see the following:



To change for the logged in user, click on the "apc" or currently logged in user option and you will see the following:


Select US Customary for Fahrenheit and Metric (default setting) for Celsius.

To change this setting for all users, Go to configuration --> security --> Local Users --> Default settings.
You will see similar settings options and again select US Customary for Fahrenheit or Metric for Celsius.
Was this helpful?
What can we do to improve the information ?