Technical FAQs

Ask a Question

Are the new 6U, 9U and 12U NetShelter cabinets hinged in the rear like the AR100 & AR100HD?

Issue:
Customers inquire if the newer 6U, 9U and 12U wall mount cabinets are hinged in the rear.

Product Line:
NetShelter WX

Environment:
All versions and serial ranges.

Cause:
The 13U NetShelter WX cabinets are hinged in the rear.

Resolution:
The new 6U, 9U and 12U NetShelter WX cabinets (AR106, AR109, AR112) are not hinged in the rear. Only the NetShelter WX AR100 and AR100HD are hinged in the rear,
Was this helpful?
What can we do to improve the information ?