Technical FAQs

Ask a Question

Uniflair: Securing Carel Leak Sensor Ribbon to the Ground

Issue:
Securing Uniflair Carel Leak Sensor Ribbon to the Ground.

Product line:
Uniflair.

Environment:
All Serial Numbers..

Cause:
Installation.

Resolution:
The Carel leak sensor ribbon provides protection across the entire strip. This allows the ribbon to be fastened by screws, silicon or by cable clamps. The ribbon may be laid on the floor or other surfaces or wrapped around pipes or flanges.

Was this helpful?
What can we do to improve the information ?