NetBotz Web Client Does Not Load When Launched from the StruxureWare Data Center Expert UI to a NetBotz Appliance on the Private LAN
Issue:
The NetBotz version 4.2 Web Client does not load completely when it is launched from the StruxureWare Data Center Expert user interface to a NetBotz appliance on the private LAN.
Product Line:
StruxureWare Data Center Expert
NetBotz
Environment:
StruxureWare Data Center Expert user interface
NetBotz version 4.2 and later Web Client
Cause:
The StruxureWare Data Center Expert proxy does not process the URL for the NetBotz Web Client.
Resolution:
Users accessing StruxureWare Data Center Expert from the public LAN must use Advanced View to connect to a NetBotz appliance on the private LAN. Alternatively, to use the Web Client, users can connect directly to a NetBotz appliance from a system on the private LAN.