Technical FAQs

Ask a Question

Display issue in NetBotz Advanced View after decreasing the image size on a Pelco camera after discovery.

Issue:

After a Pelco camera is discovered by a NetBotz appliance, decreasing the secondary image stream size on the camera causes a rendering issue.

Product Line:

NetBotz, Pelco

Environment:

NetBotz Advanced View

Cause:

The Pelco camera does not update the NetBotz appliance with the new image stream size.

Resolution:

Rebooting the NetBotz appliance should cause it to update with the new image stream size. If this does not resolve the issue, remove the Pelco camera from the NetBotz appliance, and rediscover it.
 
Was this helpful?
What can we do to improve the information ?