Technical FAQs
Technical FAQs
Issue:
What are the length of the power cords of an ACSC
Product line:
ACSC100, ACSC103
Environment:
All Product models, all serial numbers
Cause:
Resolution:
ACSC Power cord lengths
• 60 Hz unit – 5.5 Feet (1.7 m)
• 50 Hz unit – 12 Feet (3.6 m)