Technical FAQs

Ask a Question

Video: Back-UPS BX/BR "G" Manual Adjustment for Sensitivity

Issue:
Demonstration of the adjustment for the internal Sensitivity and Transfer Voltages of the Back-UPS XS/RS 'G' family.

Product Line:
BACK-UPS XS/RS

Environment: 
BX1500G / BX1500G-CA
BX1300G / BX1300G-CA
BX1000G / BX1000G-CA
BR1500G, BR1300G, BR1000G, BR700G

Cause:
Process is to adjust for frequent line issues such as Line Noise (Total Harmonic Distortion), Brownout or Over Voltage conditions. Symptom may be seen as frequent transfers
to battery power or constant "clicking" being heard from the unit.

Resolution: 
The following video details the process for manually adjusting the Back-UPS BX/BR "G" Energy Saving UPS.

Was this helpful?
What can we do to improve the information ?