Technical FAQs

Ask a Question

What are the dip switch settings for sku 5328, Apple to VGA Monitor Adapter?

Issue:
I need to connect my VGA/SVGA monitor to an Apple computer with a DB15 monitor port.  I need to know how to set the dip switches on this adapter.
 
Product Line:
Cables and Connectivity Solutions.
 
Environment:
AR5328 Apple to VGA monitor adapter. 
 
Cause:
The VGA monitor cable has a HD15 connector and the Apple computer has a DB15 port. The adapter has 6 dip switches. How are the dip switches supposed to be set?
 
Resolution :

DB15 Male to HD15 Female. Molded style 6. 10 Position DIP switch adjusting  the signal between a Macintosh Computer and IBM Monitor. Supports 6 signal  modes and resolution.
 
Monitor Resolution Mode 1 Mode 2 Mode 3 Mode 4 Mode 5 Mode 6
12"" RGB 512 x 384 1345 13456 1347 1346 13467 134
13"" RGB 640 x 480 66Hz 145 1456 147 146 1467 14
Portrait 640 x 870 2345 23456 2347 2346 23467 234
VGA/SVGA 640x 80/800x600 Hz 235 2356 237 236 2357 23
15"" Tilt 245 2456 247 246 2467 24
16"" Color 832 x 624 135 1356 137 136 1367 13
19"" Color 1024 x 768 125 1256 127 126 1267 12
21"" Color 1152 x 870 12345 123456 12347 12346 123467 1234
2 Page Mono 1152 x 870 345 3456 347 346 3467 34
NTSC 1245 12456 1247 1246 12467 124
NTSC/PAL 1235 12356 1237 1236 12367 123
HI-RES (12""-14"") 145 1456 147 146 1467 14
Multiple Scan 14"" 14589 145689 14789 14689 146789 1489
Multiple Scan 16"" 1458 14568 1478 1468 14678 148
Multiple Scan 21"" 1459 14569 1479 1469 14679 149

EXAMPLE: Mode 1345 has switches 1, 3, 4 and 5 turned on and all others turned off.
Mode SW1 SW2 SW3 SW4 SW5 SW6 SW7 SW8 SW9 SW10
1345 ON OFF ON ON ON OFF OFF OFF OFF OFF
 
MODE 1 is Composite SYNC (1) SYNC signal (DB 15M pin 3) connected to HD 15F pin 13
MODE 2 is Composite SYNC (2) DB 15 pin 3 & 15 conn. to HD 15F pin 13
MODE 3 is SYNC on V DB 15 pin 12 conn. to HD 15F pin 14
MODE 4 is SYNC on H DB 15 pin 15 conn. to HD 15F pin 13
MODE 5 is Separate SYNC DB 15 pin 12 conn. to HD 15F pin 14
DB 15 pin 15 conn. to HD 15F pin 13
MODE 6 is SYNC on GREEN SYNC on GREEN

In order to set the adapter you should know the resolution your computer is  sending to the monitor, then choose the correct setting. It may be worth a  quick check to see if the video port/card you have is SVGA compatible also. If you have a standard SVGA monitor, the video port/card is SVGA compatible,  and you don't know the resolution, this list is the most common settings.  Start at the top and work your way down the list until the video is acceptable to you.


For The Most Common SVGA Monitor Resolutions These Settings, Turn On Switches:

2,3,5,7 (supports 640 x 480 800 x 600)

1,3,6,7 (supports 832 x 624)

1,2,6,7 (supports 1024 x 768)

1,2,3,4,6,7 (supports 1152 x 870)

1,4,6,7,8,9 (multiscan 14"")

1,4,6,7,8 (multiscan 16"")

1,4,6,7,9 (multiscan 21"")
Was this helpful?
What can we do to improve the information ?