AM/PM string is not translated in scheduled reports in ISX Central 5.x
Issue:
AM/PM string is not translated in scheduled reports in ISX Central 5.x
Product Line:
InfraStruxure Central
Environment:
Version 5.1 and higher.
Cause:
AM/PM strings within the scheduled report are not translated in Russian, French, German, Portuguese, Spanish, or Italian. The reason behind this is that ISX Central is using a 12 hour clock when creating these reports and the Central currently expects the regions effected to use a 24 hour clock. There was no expectation of AM/PM translation.
Resolution:
This issue may be addressed in a future revision