Verifying Digitally Signed Pictures with Version 2 Netbotz Appliances
Issue:
Verifying Digitally Signed Pictures with Version 2 Netbotz Appliances
Product Line:
NetBotz
Environment:
NetBotz version 2
Cause:
NetBotz has included a simple command line utility that enables you to verify that digitally signed M-JPEG (AVI) files have not been tampered with since they were generated by your NetBotz appliance.
Resolution:
The file name of the command line utility is:
avivrfy.bat
It is automatically installed and can be accessed from the Advanced View installation directory.
Command Usage:
avivrfy avifilename.avi
To verify multiple AVIs,:
avivrfy sample.avi sample1.avi sample2.avi”