Technical FAQs

Ask a Question

Netbotz Advanced View Does NOT Support Radius, Active Directory or LDAP

Issue:

Netbotz Advanced View Does NOT Support Radius, Active Directory or LDAP

Product Line:

NetBotz

Environment:

NetBotz Authentication All versions

Cause:

Authentication options.

Resolution:
 
The NetBotz Advanced View does NOT support authentication or integration with Radius, OpenLDAP, Active Directory, or any remote authentication option. All authentication with the Advanced View utilizes standard username & password against the NetBotz appliance itself.

NOTE: NetBotz Central, ISX Central, and StruxureWare Data Center Expert do support integrating with both Active Directory & OpenLDAP remote authentication server software suites.
Was this helpful?
What can we do to improve the information ?