OID Information for External Humidity Sensor on Version 1 Appliances
Issue:
OID Information for External Humidity Sensor on Version 1 Appliances
Product Line:
NetBotz
Environment:
NetBotz version 1 and SNMP
Cause:
The OID information for the NetBotz External Humidity Sensor is all in the published MIB under:
iso.org.dod.internet.private.enterprises.netBotz.ExpPortTable.expPortEntry.expPort-ext-humi
Resolution:
The OID information for the NetBotz External Humidity Sensor is all in the published MIB, under iso.org.dod.internet.private.enterprises.netBotz.ExpPortTable.expPortEntry.expPort-ext-humi.
The OIDs map to:
.1.3.6.1.4.1.5528.31.1.80.1.0 (for External port 1)
.1.3.6.1.4.1.5528.31.1.80.2.0 (for External port 2)
.1.3.6.1.4.1.5528.31.1.80.3.0 (for External port 3)
.1.3.6.1.4.1.5528.31.1.80.4.0 (for External port 4)
.1.3.6.1.4.1.5528.31.1.80.5.0 (for External port 5)
.1.3.6.1.4.1.5528.31.1.80.6.0 (for External port 6)
.1.3.6.1.4.1.5528.31.1.80.7.0 (for External port 7)