Technical FAQs

Ask a Question

Symmetra Power Array redundancy alarm is limited to N+2


Symmetra Power Array has a maximum redundancy alarm limit of N+2.  The user cannot set this alarm to a value greater than 2.  This means that if the user 

Product Line

Symmetra Power Array


All serial ranges


The system is unable to support a value greater than 2 for the user configurable redundancy alarm.


The system is not capable of this function.

Please Note:
The Symmetra can report on current redundancy levels greater than N+2, such as via the PowerView Status menu or Network Management Card, etc.  The system is simply not capable of alarming when the redundancy limit falls below N+3.  This is not considered a typical use case anyway.

Was this helpful?
What can we do to improve the information ?