Enabling or disabling ISX Central Private LAN will cause server to generate a new self signed SSL certificate.
Issue:
Enabling or disabling ISX Central Private LAN will cause server to generate a new self signed SSL certificate
Product Line:
InfraStruxure Central
Environment:
InfraStruxure Central prior to 6.2
Cause:
When working with SSL certs, you will need to re-add the cert if you enable or disable DHCP on the private LAN or if you change IP information on the private LAN. This is a known issue.
Resolution:
This issue was resolved in InfraStruxure Central 6.2