Technical FAQs

Ask a Question

A file named "@LongLink" gets created in the installation path during the installation of PowerChute Network Shutdown on HP-UX.

Issue:
During installation a file named "@LongLink" gets created in the folder where PowerChute Network Shutdown 3.1 build is present and also in the /opt/APC/ folder. Because of which the APC directory is not removed after uninstallation.

Product:
PowerChute Network Shutdown version 3.1

Environment:
HP-UX 11i v3

Cause:
File creation

Solution:
issue has been address PowerChute Network Shutdown version 4.0 and above
Was this helpful?
What can we do to improve the information ?