Technical FAQs
Technical FAQs
Issue:
Can a cooling unit be tipped or laid on its side?
Product line:
All Units
Environment:
Data Center Cooling
Cause:
They absolutely cannot be laid on their sides for movement. The units also can not have any parts removed to aid in laying the unit on its side. THIS WILL VOID ALL WARRANTY. Please see below for the maximum amount of degrees that is allowed to be tipped. InRow units cannot be tipped at all due to their high center of gravity. Caution must be taken when moving these units.
ACSC10x 0
ACRC10x 0
ACRC30x 0
ACRC50x 0
ACRD10x 0
ACRD20x 0
ACRD50x 0
ACRP10x 0
ACRP50x 0
Uniflair Less than 10 Degrees
Stulz Less than 10 Degrees
FM Less than 10 Degrees
Airflow Less than 10 Degrees