GREECE - Choose Country or Region
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
Voltage Regulators
Surge Protection Devices
Filters & Harmonic Conditioners
Mobile Accessories
Portable Device Chargers
Cooling
Cooling
Cooling
Modular Access Floor
Uniflair Technical Floor
Uniflair Office Floor
Uniflair Building Floor
Air Economizers
Ecoflair Air Economizers
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
Static Transfer Switches
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
Module Optimized Cooling
Chilled Water System
Power Modules
Enclosed Power Module
Skid Mounted Power Module
IT Modules
SmartShelter Container
SmartShelter Module
SmartShelter Data Hall
SmartShelter Room
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
Data Center Assessment Services
Install
Installation Services
Network Integration
Operate
Remote Monitoring Services
Battery Replacement Services
Extended Warranties
Preventive Maintenance
Service Plans
Optimize
Training Services
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
GREECE - Choose Country or Region
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
Migration from ISX Manager to ISX Central hangs on Private Network Check.
Issue:
Migration from ISX Manager to ISX Central hangs on Private Network Check.
Product Line:
InfraStruxure Central / StruxureWare Data Center Expert
Environment:
Potentially all versions
Cause:
IP scheme mis-configuration
Resolution:
If you set up the private side IPs of ISX manager and ISX Central similar to the following, you will see the aforementioned issue:
Manager's private network configuration: IP: 192.168.0.1 Subnet: 255.255.252.0 (therefore the network range was 192.168.0.0-192.168.3.254
Central's private network configuration:IP: 192.168.3.254 Subnet: 255.255.254.0 (network range 192.168.2.0 to 192.168.3.254) DHCP turned off.
To resolve the issue, change the IP scheme so that they match.