Technical FAQs

Ask a Question

How can I identify what Server Modules are connected to my KVM (AP5602, AP5610, AP5615, AP5616) through the KVM interface?

Issue

How can I identify what Server Modules are connected to my KVM (AP5602, AP5610, AP5615, AP5616) through the KVM interface?


Product Line
 

  • Rack Accessories - KVM Switches
    • AP5602
    • AP5610
    • AP5615
    • AP5616



Environment

  • All serial numbers
  • All firmware versions



Cause

This information is provided for general reference.


Resolution


Note: This ONLY applies to the AP5602, AP5610, AP5615 and AP5616

In the KVM’s web interface home screen (connection page) you should see all of your connected servers. Under the EID column on that page you should see a 12 digit number divided in half by a hyphen (ex. 520705-0000A2). The first 6 digits of that number refer to the physical ID of the Server module that is being used. Reference the EID chart below for easy translation:

 

Model

EID Description
 AP5630 520705 APC KVM PS/2 Server Module  
 AP5631 520706 APC KVM USB Server Module 
 AP5632 520707 APC KVM SUN Server Module 
 AP5634 520709  APC KVM USB VM Server Module 
 AP5635 520710 APC KVM PS/2 VM Server Module
 AP5636 520713 APC KVM VT100 Serial Server Module  
 AP5602 520698 APC 16-Port Cat5 KVM (0x2x16)
 AP5610 520701 APC 16-Port IP KVM (2x1x16)
 AP5615 520703 APC 32-Port IP KVM (2x1x32)
 AP5616 520704 APC 32-Port IP KVM (8x1x32)


 
Was this helpful?
What can we do to improve the information ?