Technical FAQs

Ask a Question

Why does my NetBotz Smoke Alarm stay on, even when the smoke has cleared?

Issue:
Why does my NetBotz Smoke Alarm stay on, even when the smoke has cleared?

Product Line:
NetBotz

Environment: 
NetBotz 
NBES0307 (Smoke Sensor)

Resolution:

The NetBotz Smoke is designed to stay in alert even after the smoke is gone. A reboot of the NetBotz Appliance or at at least disconnecting and reconnecting the sensor will clear the alarm.
This is by design.
Was this helpful?
What can we do to improve the information ?