Video: How do I customize short message e-mail alarm actions in Data Center Expert?
Issue:
Customizing short message e-mail alarm actions in StruxureWare Data Center Expert
Product Line:
StruxureWare Data Center Expert (DCE)
Environment:
StruxureWare Data Center Expert (DCE)
Cause:
E-mail notifications from DCE come in a pre-defined format that can not be edited. To customize e-mail notifications, short message e-mail alert actions need to be used.
Resolution:
1) Open the DCE Client and go to: Alarm Configuration menu > Manage Alarm Actions.
2) Click on Create and then select Short Message E-Mail. Select Next.
3) Provide an Action Name and add in the e-mail addresses that this alarm action will be sent to.
4) The subject and message fields can be customized using a defined list of macros, which are available on https://dcimsupport.apc.com.