Technical FAQs

Ask a Question

What is the maximum roof load rating for NetShelter SX and SV cabinets?

Issue:
The maximum load rating for the roof is needed.

Product Line:
NetShelter SX, NetShelter SV

Environment:
All versions and serial ranges.

Cause:
Customers need to know the load rating to make sure it's not exceeded.

Resolution:
The roof of both the NetShelter SX and SV cabinets is rated to 200 lbs.
Was this helpful?
What can we do to improve the information ?