Technical FAQs

Ask a Question

Version 2 NetBotz ​0-5V sensor on Sensor Pod 120 reports double the actual voltage in Advanced View


Issue:
0-5V sensors connected to the NetBotz Sensor Pod 120 with the NetBotz 0-5V Sensor Cable (NBAC0231) report double the actual voltage in Botzware and the Advanced View.

Product Line:
NetBotz

Environment:
Advanced View v4.3 and 4.4
NetBotz 0-5V Cable (NBAC0231)

Cause:
Firmware updates affected the performance of the NetBotz 0-5V Cable (NBAC0231).

Resolution:
There is no resolution at this time.
Was this helpful?
What can we do to improve the information ?