Issue:
DIN Connector Pin Outs For the Netbotz Appliances
Product Line:
NetBotz
Environment:
NetBotz version 1 and 2 cables
Cause:
Pin-out specifications.
Resolution:
DIN Connector Pin Outs
-NetBotz does not release the pin outs for the DIN connectors for any NetBotz Appliances.
-To address this issue, NetBotz sells a standard dry contact cable that is our DIN connector one end and two bare dry contact style wires on the other.
-This cable is provided to allow customers to attach our NetBotz Appliances to any dry contact type connection without having to have the DIN connector pin outs.