Technical FAQs

Ask a Question

Details Returned from NetBotz Devices via Advanced Device Crawlers

Issue:

Details Returned from NetBotz Devices via Advanced Device Crawlers

Product Line:

NetBotz

Environment:

NetBotz version 2 Advanced Device Crawlers.

Cause:

The following information can be queried via Advanced Device Crawlers for NetBotz appliances assuming the NetBotz DDF (Device Definition File) is installed on the server appliance and the client appliance is SNMP enabled. Please note that not all information listed below is available on all NetBotz models.

Resolution:

 
  • Model
  • Temperature
  • Humidity
  • Airflow
  • Audio Alarm
  • Door Switch
  • Camera Motion
Was this helpful?
What can we do to improve the information ?