Technical FAQs

Ask a Question

Netbotz External Temperature Sensor Operating Range

Issue:

Netbotz External Temperature Sensor Operating Range

Product Line:

NetBotz

Environment:

NetBotz version 2 sensor TS100

Cause:

Product information

Resolution:

External Temperature Sensor Operating Range 

The external temperature sensor range (TS100) is:

-30 to +60 degrees C
-20 t0 +140 degrees F

Was this helpful?
What can we do to improve the information ?