Technical FAQs

Ask a Question

NetBotz Central 2.x - Graph Color Legend are Incorrect

Issue:

NetBotz Central - Graph Color Legend are Incorrect

Product Line:

NetBotz Central

Environment:

NetBotz Central 2.x

Cause:

When color boxes in the table of a graph view are all white boxes, users cannot distinguish which line corresponds to which sensor

Resolution:


This is typically tied to the client settings, and can usually be corrected by going to "Edit->Preferences", then in "Appearance" switch to a non-Windows "Look and Feel" (In NBC v2.1.x, it is called "Toolbar"), and close and re-open the NetBotz Central console.
 
Was this helpful?
What can we do to improve the information ?