Technical FAQs

Ask a Question

Symmetra LX and the InfrastruXure (ISX) Manager Load Reports


Issue

Symmetra LX and the InfrastruXure (ISX) Manager Load Reports - what to expect


Product Line
 
  • InfrastruXure (ISX) Manager - AP92200
  • Symmetra LX UPS Models

Environment
  • Using ISX Manager reporting
  • All ISX Manager versions

Cause


The Symmetra LX is a split-phase UPS which reports an individual value for load percentage on each of the two "hot" legs that are present.


Resolution


Since the output of multiple phases is being monitored and recorded, the Symmetra LX will appear in the "3-Phase UPS Load" report in ISX Manager and not on the "1-Phase Load" report as is the case with other Symmetras. The third phase in this report will be reported as "Unknown."
 
Was this helpful?
What can we do to improve the information ?