Technical FAQs

Ask a Question

What are the supported SNMP OIDs for APC products? Where can I download the APC SNMP MIB?


Issue

  • What are the supported SNMP OIDs for APC products?
  • Where can I download the APC SNMP MIB?



Product Line

Simple Network Management Protocol (SNMP) Enabled APC Products excluding most NetBotz products (except NetBotz 200).


Environment


  • All serial numbers
  • All firmware versions

Cause

For SNMP connectivity and Object Identifiers (OIDs), the APC PowerNet MIB file is required. Please see below.


Resolution

The APC Powernet reference guide for all supported products can be downloaded here:

http://www.apcmedia.com/salestools/ASTE-6Z5QEY/ASTE-6Z5QEY_R0_EN.pdf

The APC PowerNet MIB can be downloaded here: http://www.apc.com/tools/download/index.cfm

Select Firmware Upgrades - MIB from the Filter By Software / Firmware drop down list and press Submit.

The Powernet MIB supports all APC network enabled devices except Netbotz. NetBotz has a dedicated SNMP MIB (excluding NetBotz 200).

Please note that as of v5.1.7 and higher , the sumx and sy applications also have support for the RFC1628 Generic UPS MIB. Please refer to knowledge base FA156148 for additional information and recommendations regarding SNMP MIB use.


Was this helpful?
What can we do to improve the information ?