Technical FAQs

Ask a Question

Is there a minimum load rating for the NetShelter SP cabinets?

Issue: 
Customers may ask if there is a minimum load rating needed before moving to Shock Packaging. 

Product Line: 
NetShelter SX Shock Package

Environment: 
All models, all serial numbers. 

Cause: 
Customers may need to ship cabinets with a light load, and ask if there's a load weight at which we recommend Shock Packaging be used. 

Resolution:
We recommend Shock Packaging cabinets be used when shipping cabinets loaded, regardless of the weight. 
Was this helpful?
What can we do to improve the information ?