Can not discover Servertech PDU in StruxureWare DCE using SNMP version 3
Issue:
Can not discover Servertech PDU in StruxureWare DCE using SNMP version 3
Product Line:
StruxureWare Data Canter Expert
Environment:
StruxureWare DCE (potentially any version)
SNMP version 3
Servertech PDU (CW-24VYM311A1, potentially others)
Cause:
Potential configuration issue on the Servertech PDU. Device not discovering in SNMP version 3 if authentication is set.
Resolution:
During discovery in DCE, it was seen that changing the "trap type" on the PDU to snmpv3 allowed DCE to discover the device. Please also note that during discovery of 3rd party devices, the priority scanning" option should be unchecked.