Technical FAQs

Ask a Question

How to configure PowerChute Personal Edition to recognize French language OS.

Issue:
How to configure PowerChute Personal Edition to recognize French language OS.

Product Line:
PowerChute Personal Edition version 3.X

Environment:
All support Windows OS

Cause:
Installation to non English language OS.

Solution:
To install PowerChute Personal Edition for a non English base OS the OS must be set for the desired language prior to PowerChute being installed. 

NOTE: To install the French version of PowerChute the OS must be set to French  - France. If the system is set to French - Canada the program will run in English. 

To change the system language settings go to Control Panel, Region and Language



Set format to French (France) and click apply to install the French version of PowerChute Personal Edition



Change Location to France and click apply



 
Was this helpful?
What can we do to improve the information ?