Technical FAQs

Ask a Question

"BIOS is Already Bypass Error on Adapter 0." message when restoring a Data Center Expert Enterprise server

Issue:
"BIOS is Already Bypass Error on Adapter 0." error is displayed when imaging a StruxureWare Data Center Expert Enterprise server from the v7.2.6 restore.iso:

Product Line:
StruxureWare Data Center Expert

Environment:
StruxureWare Data Center Expert v7.2.6 Enterprise server

Cause:
This informational message indicates the adapter is already in Bypass Error mode, a normal part of the restore process. 

Resolution:
The 0 exit code indicates the error is harmless and can be overlooked.
Was this helpful?
What can we do to improve the information ?