Can the NetShelter SX cabinet be purchased with no sides, doors, roof or other configuration?
Issue:
Customers may want to buy a NetShelter SX cabinet without sides, doors, roof, etc
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
Customers may not need certain features of the standard NetShelter SX cabinet.
Resolution :
NetShelter SX cabinets are available in custom configurations. The most common configurations already have part numbers called X-options.
The X-option part number is added to the end of the standard sku.
X609 = No Sides
X610 = No Doors
X617 = No Sides, No Doors
EXAMPLE:
An AR3100 with no sides is AR3100X609.
An AR3100 with no doors is AR3100X610.
An AR3100 with no sides or doors is AR3100X617.
For other custom configurations please contact APC.