GHANA - Choose Country or Region
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
Voltage Regulators
Surge Protection Devices
Filters & Harmonic Conditioners
Mobile Accessories
Portable Device Chargers
Cooling
Cooling
Cooling
Modular Access Floor
Uniflair Technical Floor
Uniflair Office Floor
Uniflair Building Floor
Air Economizers
Ecoflair Air Economizers
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
Static Transfer Switches
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
Module Optimized Cooling
Chilled Water System
Power Modules
Enclosed Power Module
Skid Mounted Power Module
IT Modules
SmartShelter Container
SmartShelter Module
SmartShelter Data Hall
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
Data Center Assessment Services
Install
Installation Services
Operate
Battery Replacement Services
Extended Warranties
Preventive Maintenance
Service Plans
Optimize
Training Services
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
GHANA - Choose Country or Region
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
GPS Receiver Support for the NetBotz 500
Issue:
GPS Receiver Support for the NetBotz 500
Product Line:
NetBotz
Environment:
Version 2 NetBotz 500
Cause:
Supported configurations..
Resolution:
The NetBotz 500 supports the attachment of a GPS (global positioning system) receiver.
The NetBotz 500 reports GPS readings such as latitude, longitude, altitude, heading, velocity, and status as monitorable sensors
Current latitude and longitude readings can be attached to all alerts
Connects to WB500 USB port using USB-to-RS232 serial converter cable
Support for two NMEA-compliant GPS receivers:
Garmin GPS35 USB
Laipac G10-USB