Technical FAQs

Ask a Question

Contents of the Mounting Kit Included with the Models 320 & 420

Issue:

Contents of the Mounting Kit Included with the Models 320 & 420

Product Line:

NetBotz

Environment:

NetBotz 320 & 420

Cause:

N/A

Resolution:

The following items are included in the mounting kits:

Black universal swivel wall mount (plastic)
3 anchors (1"" long)(suitable for concrete) and 3 anchors (1-1/2"" long)(for sheet rock).
4 screws (#6 x 1/4"", phillips)
5 black tie wraps (7-1/2"" long) and 4 platforms (adhesive; can be stuck on walls; used with the tie wraps). 
Was this helpful?
What can we do to improve the information ?