Technical FAQs

Ask a Question

Galaxy VX; Customer, consultant or engineer looking for the center of gravity (CoG) for the IO and/or PC enclosures

 
 
Issue:
Customer, consultant or engineer looking for the Center of Gravity (CoG) for the IO and/or PC enclosures.
 

Product line:
Galaxy VX
 

Environment:
All models, all serial numbers
 

Cause:
none.
 

Resolution:
The enclosures have the following CoG.
 
  • GVX PC: X-distance 290mm, Y-distance 930mm , Z-distance 440mm
 
  • GVX 750kW IOC: X-distance 590mm, Y-distance 830mm, Z-distance 390mm
 
  • GVX 1000kW IOC: X-distance 590mm, Y-distance 830mm, Z-distance 390mm
 
  • GVX 1500kW IOC: X-distance 1060mm, Y-distance 970mm, Z-distance 430mm
 
  • GVXMBCR750: X-distance 399.7mm, Y-distance 993mm, Z-distance 471.5mm
 
(X=width, Y=height, Z=depth)
 
 

 
Was this helpful?
What can we do to improve the information ?