Technical FAQs

Ask a Question

Questions on where to ship 3 phase batteries for disposal

Issue:
Questions on where to ship 3 phase batteries for disposal
 
Product line:
3 Phase cartridge batteries
 
Environment:
All 3 phase modular battery units.
 
 
Resolution:
Customers can ship batteries to the following address for proper disposal of 3 phase related batteries –
 
Schneider Electric
201 Fulling Mill Rd, Middletown, PA 17057 
 
 
  • For all 3 phase batteries the customer is required to pay for the return ship of any battery that is not under warranty or specific Battery Service contracts.
  • Customers may arrange their own heavy weight pick up if desired thru major shipping companies.
  • Schneider does not provide packaging for returning batteries. 


 
Was this helpful?
What can we do to improve the information ?