Technical FAQs

Ask a Question

Is there documentation available that shows the rackmount depths for Dell products?

Some Dell products have mounting rails that interfere with a PDU, or mount so deep that the rear doors won't shut.

Product Line:
NetShelter SX

All versions and serial ranges.

Some Dell products extend beyond the rear mounting rails of the cabinet, and also have cable management that intrudes even further into the rear of the cabinet.

The attached file is a web page from Dell that shows many Dell rackmount products, optional rail kits and their optional cable arms. This document shows the overall mounting depths of these various rail kits and their options. There is also a section that has other notes regarding compatibility of these rail kits, specific to the NetShelter SX 600mm W x 1070mm D cabinets.
This document was found at:
See attached file.
Was this helpful?
What can we do to improve the information ?