Technical FAQs

Ask a Question

Do the 2G series PDUs fit into the NetShelter VX cabinets?

Issue:
Some of the newer rPDUs like the 2G are longer and may not fit into the older cabinet designs like the VX.

Product Line:
NetShelter VX

Environment:
All versions and serial ranges.

Cause:
Customers need to know that the rPDU they are purchasing will fit into their NetShelter VX cabinet.

Resolution:
Please use Knowledge Base document FA158651 to find compatibility between all rPDUs and cabinets.
The Knowledge base is available from the FAQ page of the APC website: http://www.apc.com/us/en/gd/en/faqs/content/?id=FA158651 

  • FA158651 contains a document which shows all current NetShelter cabinets and the products that can be installed into them.
  • Open the file and scan down until you reach the PDU section. Find the PDU in question. 
  • Then, scan to the right until you reach the correct NetShelter cabinet. If the two are compatible there will be a checkmark.
Was this helpful?
What can we do to improve the information ?