Information overwritten if two InfraStruXure Central servers use the same remote repository.
Issue:
Information overwritten if two InfraStruXure Central servers use the same remote repository
Product Line:
StruxureWare Central / Data Center Expert
Environment:
StruxureWare Central any version
Cause:
If you add a remote repository that is already been used by another ISX Central server, the repository.id file is overwritten (which contains the Mac address of the server and mounted date). This may cause problems if multiple servers are using the same remote share.
Resolution:
Each StruxureWare system needs it's own unique repository/shared folder.