Technical FAQs

Ask a Question

How do I enable Telnet on a version 2 or 3 NetBotz appliance?

Issue:

Enabling Telnet on a version 2 or 3 NetBotz appliance

Product Line:

NetBotz

Environment:

NetBotz version 2 and 3

Cause:

Alternate configurations

Resolution:

Telnet is disabled on a Version 2 and 3 NetBotz Appliances by default, and in order to turn it on use the following procedure.

To enable telnet temporarily, simply type in the following URL in a web browser:
http://ip-of-appliance/enabletelnet

To disable telnet, simply type in the following URL in a web browser:
http://ip-of-appliance/disabletelnet

Upon reboot, the appliance will disable telnet again, in other words, it`s not a persistent setting.
 
Was this helpful?
What can we do to improve the information ?