A system defect discovered in NetBotz Central 2.x could potentially affect the performance of your NetBotz Central system. A defect has been found in NetBotz Central version 2.x that may prevent you from upgrading your NetBotz Central 2.x system via the internet. Furthermore, this defect could cause a large amount of free space on the data volume of your NetBotz Central to be consumed with a large temporary file.
Resolution:
To address this issue, NetBotz has released NetBotz Central 2.0.3. It is currently available from NetBotz. Since this defect affects the internet upgrade, you must upgrade your NetBotz Central using a CD. The NetBotz Central 2.0.3 Upgrade CD may be obtained by downloading the ISO CD-ROM image. Once the CD-ROM image is downloaded, a CD may then be burned for use in upgraded NetBotz Central. If you are unable burn CD's from ISO CD-ROM images, NetBotz will be happy to ship you copy of the NetBotz Central 2.0.3 Upgrade CD.
It is very important that you upgrade your NetBotz Central to version 2.0.3 as soon as possible. Please contact NetBotz Technical Support for more information on obtaining the Upgrade CD’s. NetBotz Technical Support may be contacted via: